An early warning system for production

Winterthur, 17 July 2018 – Piezoelectric strain sensors from Kistler safeguard machines against overload and help to achieve precise monitoring of the stresses on tools in produc-tion sectors where technologies such as punching, forming and joining are used. Simple installation and wide measuring ranges make these sensors ideal for retrofitting on existing plants.

With advances in digitization as we move towards Industry 4.0, sensors are gaining more and more ground in industrial manufacturing – even conquering sectors where the processes are mainly me-chanical. Examples include punching and press-fit technologies as well as forming and joining processes. When the aim is to increase the options for monitoring processes such as these, strain sensors are an excellent solution: they can either be mounted directly on the machine or integrated into tools as measuring pins.

Anything but superficial

Piezoelectric (PE) surface strain sensors from Kistler deliver high-resolution measurements of the strain in a structure. The strain is transmitted to the measuring element as a shear force, via static friction. Measurements feature long-term stability (with no creep), and these rugged sensors are protected against overloading (degree of protection: IP67) and resistant to interference from disturbance variables such as temperature influences.

Thanks to their extremely compact design, the sensors can be fixed directly onto the machine in the appropriate position with just one screw. If irregular force peaks occur, they are registered immedi-ately with no risk of the sensors themselves being damaged – in case of overload, they 'slide' on the surface until the strain is relieved. It makes no difference whether the forces occurring are very small or very large – thanks to their high natural frequency and wide measuring range, these sensors can cope with both. Piezoelectric surface strain sensors from Kistler therefore act as an early warning system, delivering effective machine protection that helps to reduce costly downtime.

Tool monitoring made easy

Sometimes there is also a requirement to obtain valuable process data on individual assembly steps. To meet this need, Kistler also offers strain sensors that can be integrated directly into the tool as measuring pins. This option offers effective monitoring and optimization for applications in punching and forming technology, among others. Kistler's highly sensitive measuring pins detect the smallest deformations of the material, even under highly dynamic and quasi-static loads.

Integration in the tool requires a cylindrical bore hole in which the measuring pin is preloaded with axial or radial alignment. In this way, extension and deflection can be measured either longitudinally or transversely to the sensor. Measuring pins are mainly used where the conditions are not suitable for a measurement on the surface, or the installation space is very limited.

Digital signal evaluation simplifies the measurement chain

As from the start of this year, Kistler is offering the 5074A charge amplifier which digitizes PE signals: for the first time ever, users can now integrate any desired piezoelectric sensors into the control environment. Thus, customers now have the opportunity to connect PE strain sensors with the machine control via Industrial Ethernet. There is no longer any need for the detour via an analog evaluation system, and networking with higher-level systems is simplified – a quantum leap towards Industry 4.0 and the industrial Internet of Things.

For more information on strain sensor technology from Kistler, visit:
https://www.kistler.com/en/applications/industrial-process-control/process-monitoring-forming/

Press kit

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

10/16/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
10/8/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
9/24/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
9/21/2018
At Fakuma 2018, Vester will showcase all the benefits of automated testing
9/17/2018
Top performance, team spirit and passionate commitment are qualities shared by Tigers Tübingen and the Kistler Group.
9/10/2018
High-accuracy dynamometer combined with innovative chuck extends tool lifetime and reduces production costs
9/6/2018
Machinery manufacturer LIK joins the Kistler Group, opening up wider access to the electric vehicle market
8/28/2018
Enhanced transparency in plastics processing
8/21/2018
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
8/21/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
7/31/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
7/25/2018
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
7/18/2018
Effective monitoring with strain sensors protects machines and tools
7/3/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises (SMEs) for the 10th time.
6/25/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
6/19/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
6/11/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
5/11/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
5/9/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
5/8/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
5/3/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
4/24/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
4/12/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
3/6/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2/16/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2/15/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
1/31/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
1/24/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
1/23/2018
Overcoming the complexities of RTM – with Kistler
10/12/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor technology and test automation.
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality assurance in injection molds.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
10/21/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
10/19/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
9/30/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
9/7/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
7/24/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
7/12/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
5/12/2016
Screw technology complements the range of applications.
4/27/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and rehabilitation.
4/22/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
11/10/2014
New product developments for dynamic measuring technology at the Kistler booth at SPS IPC Drives 2014
10/14/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data of CoMo Injection Systems
9/29/2014
Users obtain a full range of force–displacement measurement systems from one source
6/3/2014
Extending the maXYmos product range to control and monitor production processes and quality assurance
5/26/2014
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
5/19/2014
Users obtain a full range of force–displacement measurement systems from one source
2/6/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.