Kistler Showcases Solutions for Dependable Bolted Joints

Winterthur, 27 October 2016 – At this year's SPS IPC Drives in Nuremberg from 22 to 24 November, Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment and test systems for torque tools, as well as measuring systems for random sample testing. Among the products on show at the stand, the spotlight is on INSPECTpro – the new monitoring system to measure torque and rotation angle – along with cutting-edge products from Kistler's joining and torque portfolio.

In automated production, everything revolves around accurate, reliable process monitoring. Especially in the automotive industry, monitoring and control of bolted joints is hugely important for quality assurance. That's because all the influences that find their way into this process converge at the end of the process chain. Even the smallest errors in the development or assembly process can cause costs running into millions. By integrating Schatz GmbH into the Kistler Group, Kistler is deepening its application know-how in bolted joint technology – so for the first time, customers across the globe have access to bolted joint expertise from one single source.

INSPECTpro for More Transparent Testing Processes

INSPECTpro, the portable measuring device for torque and rotation angle, opens up new possibilities in terms of hardware as well as software: now, process capability checks and random sample inspections during assembly are even easier to perform. Graphic analyses of assembly processes ensure optimal quality in bolted joint assembly. Customers always need testing to be faster and more effective, so new software modules are constantly being developed to ensure easier handling for users and greater transparency in test processes. One new feature is the Tool Management license. Tools to be tested can be stored here ahead of time so they can be conveniently called up later on in Tool Testing mode. The Tolerance Classes software module handles the use of stored tolerance classes in the parameter sets for tool testing/management or bolted joint management.

NCFR – Dynamic Drive Technology and High-Precision Sensors

The latest products from Kistler's range of joining modules will also be on show at the stand: Kistler is presenting its NCFR Joining Module – as well as the classical linear joining process, this system can perform a controlled rotary movement of the ram, either sequentially or even simultaneously. Like the entire family of NC joining systems, the NCFR joining module features a variety of additional benefits: users will appreciate its enormous flexibility and excellent dynamics combined with intuitive operation – so joining processes ranging from simple to highly complex can be handled rapidly and efficiently. Thanks to the servo amplifiers used, all traverse movements that are performed can be controlled with high precision.

Torque Sensor 4503B and KiTorq 4550A: Sensor Technology for Maximum Precision

The cutting-edge sensor technology showcased by Kistler at the SPS IPC Drives in Nuremberg will convince visitors that our company also represents the state-of-the-art when it comes to the development of high-precision torque sensors. The 4503B torque sensor offers a host of extended functionalities, bringing it into line with the very latest market requirements. For instance, optical speed and angle sensing has now been replaced by magnetic technology. This gives the sensor the advantage of added resilience for reliable operation in heavily contaminated industrial environments (e.g. where oil mist is present) – thereby saving valuable time on maintenance. The torque sensor's electronics have also been optimized, and the 4503B now has a cut-off frequency of 10 kHz for highly dynamic measurements.

Another technological milestone on Kistler's stand is the KiTorq 4550A with angle sensing – to enable determination of torque, speed or rotation angle with exceptionally high resolution (up to 8192 pulses per revolution). The number of pulses can be freely adjusted to the requirements as appropriate.

The torque measuring flange system consists of a measuring element, the KiTorq rotor and a torque evaluation unit (the KiTorq stator). With a suitable selection of components for the specific test bench, this system offers excellent flexibility for manufacturers of electrical motors and combustion engines, transmissions, pumps and compressors: this is because the ringless stator makes it possible to use different measuring elements without having to rebuild the entire test setup.

maXYmos TL 1.2 and maXYmos BL 2.3: the Latest Generation of Monitoring Systems

Kistler's stand also highlights the latest generation of maXYmos monitoring systems. Their purpose: to deliver consistent, process-integrated quality assurance. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. Because this control is integrated in the process, the system provides the basis for enhanced transparency in assembly and testing systems – paving the way for increased costefficiencythroughout the production facility. 

Don't miss the trade show date!

If you want to see Kistler's diverse range of solutions for interconnected quality monitoring at first hand, save the dates for the SPS IPC Drives trade show now: it runs from 22 to 24 November 2016 in Nuremberg.



Media Contact:
Simone Koch
Divisional Marketing Manager IPC
Phone: +41 52 224 18 02
Email: simone.koch@kistler.com

Press kit

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

7/31/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
7/25/2018
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
7/18/2018
Effective monitoring with strain sensors protects machines and tools
7/3/2018
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises (SMEs) for the 10th time.
6/25/2018
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
6/19/2018
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
6/11/2018
Kistler is earmarking the highest investment budget for research and development in the company`s history.
5/11/2018
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
5/9/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
5/8/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
5/3/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
4/24/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
4/12/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
3/6/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2/16/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2/15/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
1/31/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
1/24/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
1/23/2018
Overcoming the complexities of RTM – with Kistler
10/12/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor technology and test automation.
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality assurance in injection molds.
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
10/27/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment, torque tools test systems and more.
10/21/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
10/19/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
9/30/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
9/7/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
7/24/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
7/12/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
5/12/2016
Screw technology complements the range of applications.
4/27/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and rehabilitation.
4/22/2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
11/10/2014
New product developments for dynamic measuring technology at the Kistler booth at SPS IPC Drives 2014
10/14/2014
Wide range of options for optimizing the quality assurance through documenting and evaluating production data of CoMo Injection Systems
9/29/2014
Users obtain a full range of force–displacement measurement systems from one source
6/3/2014
Extending the maXYmos product range to control and monitor production processes and quality assurance
5/26/2014
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
5/19/2014
Users obtain a full range of force–displacement measurement systems from one source
2/6/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.