Kistler showcases practical sensor integration for injection molds

Winterthur, 25 April 2017 – At the second international Moulding Expo in Stuttgart (from 30 May until 2 June 2017), the Kistler Group will show how easy it is to install the measurement technology needed for quality assurance in injection molds. As well as offering visitors the chance to try out a realistic example of this technology, Kistler's stand at the international trade fair will focus on two product groups that feature new developments: sensors that are insensitive to their installation position and multichannel connectors.

Sensor technology has to be integrated into molds in order to optimize the injection molding process. Growing numbers of injection molders see this as an essential requirement to prepare them for the 'digital revolution' – and to raise their product and process quality to new levels. Kistler identified this need at an early stage and at the Moulding Expo, the Group will showcase its solutions and tools designed specifically so that moldmakers can meet the requirements for integrated quality testing in the injection molding process.

Hands-on! Sensor installation in six steps

At Kistler's stand E61 in hall 5, customers and visitors can try this technology out for themselves and learn how easy it is to integrate Kistler's sensors into injection molds. In six steps, we'll show you how sensors are positioned, installed, cabled and function-tested. Kistler is constantly working to make it as simple as possible for moldmakers to integrate measurement technology into their processes. As well as special tools and an extensive range of accessories, the Swiss specialist offers practical support through worldwide service and training units on installation, commissioning and maintenance.

Multi-channel connector – with added new features

With the new Type 1722 multi-channel connectors, up to eight sensors can easily be linked up via single-wire plug connections – so there's no need for screwed joints, and the connector is more robust. The new, completely redesigned connecting elements ensure simple, error-tolerant installation and what's more, they are backwards-compatible with the predecessor version as regards con-nections and space requirements. Whether the four-channel or eight-channel version is used, changing the connection elements is a straightforward operation. This technology also enables combined pressure/temperature measurements (with the help of an additional thermocouple amplifier).

Installation made simple – because the sensor is insensitive to its installation position

Cavity pressure is one of the key factors in the injection molding process. Piezoelectric sensors from Kistler allow you to capture long-term measurements of this variable with high linearity, independently of temperature: a critical contribution to quality assurance. Depending on the installation conditions, part geometries and plastic materials, Kistler offers a wide choice of variants for direct in-cavity measurements, indirect and contact-free measurements, or combinations for contact tem-perature measurement.

At the Moulding Expo 2017, Kistler will unveil its new Type 6185 sensor, which is insensitive to its installation position. This product has been systematically adapted to confined installation conditions – its frontal diameter is a mere 2 mm – and its design ensures that measurement results cannot be falsified by lateral forces (such as those caused by difficult installation conditions). The results: maximum precision with simplified installation. With this sensor too, signal transmission can be implemented with a conductive spacer sleeve instead of via cables.

Piezoelectric sensor technology: the basis for process monitoring

To be sure that their machines will meet the requirements of the future, more and more manufacturers are turning to integrated quality assurance in the injection molding process. Kistler's ComoNeo monitoring system offers a reliable solution for monitoring cavity pressure and forecasting part quality. However, there is one key requirement for the sought-after goal of zero-defect production: sensor technology must be suitably integrated at mold level. The Kistler Group will demonstrate the wide-ranging options for achieving this goal – and will highlight some points to note during installation – at the trade fair in Stuttgart from 30 May until 2 June. Anyone interested is warmly invited to visit stand E61 in hall 5 at the fair.

Media Contact:
Simone Koch
Divisional Marketing Manager IPC
Phone: +41 52 224 18 02
Email: simone.koch@kistler.com

Press kit

Kistler portrait with logo for a quick overview: Kistler Press Kit.zip

4/12/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
3/6/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
2/16/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
2/15/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities...
1/31/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint...
1/24/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
1/23/2018
Overcoming the complexities of RTM – with Kistler
10/12/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
10/27/2016
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
10/21/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
10/19/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
9/30/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
9/7/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
7/24/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
7/12/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
5/12/2016
Screw technology complements the range of applications.
4/27/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...