High-precision measurement data for the optimization of cooling lubricants

Blaser Swisslube AG, located in Hasle-Rüegsau, is a leading manufacturer of lubricants for metal parts manufacturing. In the development of new cooling lubricants, the Swiss company relies on Kistler's measurement expertise. High-precision measurement data ensures that the cooling lubricants are adapted exactly to the application requirements and that they function reliably in practical use.

More than Eighty specialists, research and experiment engineers at Blaser Swisslube are located in the Development and Technology center, with the goal to solve present and future challenges. The development of new machines, materials and processes leads to new application areas for cooling lubricants and, thus, to new challenges. To address these challenges, the properties of newly developed cooling lubricants are tested and optimized. Blaser Swisslube generates measurement data under industrial operating conditions with the goal of recording a wide range of parameters for analysis of cooling and lubricating behavior.

Because cutting force components are directly related to the tribological ratios in the cutting zone, recording these components is very important in assessing new lubricant recipes. This information can be used to gain detailed knowledge of the lubricating properties of a cooling lubricant and its constituent parts as well as to analyze the influences of the cooling lubricant with increasing tool wear. The demands on the dynamics and accuracy of the measuring system are likewise correspondingly high. It is important that the stability in the cutting process not be negatively influenced. The conditions of industrial production can thereby be maintained and valid measurement results obtained. For measurements in this extreme range, a very rigid and compact measuring system must be used.

The Kistler 3-component measuring system 9129A is used in the measurements performed by Blaser Swisslube. The instrument satisfies all requirements with respect to accuracy, dynamics and very high rigidity. Furthermore, it is compact and can be installed directly in the machine without significant effort. The system is used in all cutting tests on the lathe and delivers reliable data on cutting force, feed force and passive force. Thanks to the piezo technology that is used, the measuring range and the resolution can easily be adapted to the respective application without changing the stability of the system.

By constantly recording the force, Blaser Swisslube is able to compare cooling lubricants and their constituent parts.

Depending on the cooling lubricant technology, the force distributions vary greatly. Together with other modern measurement tools, we are thereby able to exactly record the mechanisms of action of the cooling lubricant in the cutting process."

Manfred Schneeberger, process engineering manager at Blaser Swisslube AG

 

The Development department benefits from the knowledge gained: future cooling lubricant solutions can be even more precisely tailored to the respective requirements.

7/16/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by...
4/11/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks...
11/14/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
8/11/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint...
1/4/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase...
12/22/2016
Kistler makes progress in vehicle development possible
12/22/2016
Kistler Sensor Correvit® SFII measures world record
12/20/2016
Kistler sensors deliver a maximum in data quality under any conditions.
11/7/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
10/5/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
8/17/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2/19/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
11/4/2015
Piezoelectric Measurements with CompactRIO™
6/15/2015
Measurement Solutions for Automotive Test Systems
5/8/2015
Quality Assurance in the Automotive Industry
3/2/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
12/2/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions...
12/2/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface...
8/23/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
2/15/2011
End-to-end process monitoring for critical medical moldings
2/7/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact