BIG Daishowa relies on cutting force measurement from Kistler for superior tool development

BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.

More than 500 machine tools as well as some 300 robots and automated systems — these are the figures for BIG Daishowa’s production capacity. The family-owned company was founded in 1967 and employs close to 900 employees worldwide. In Europe and North America the company is known through its subsidiary, BIG KAISER. The core competence of BIG Daishowa: high-quality tool holders for cutting with a machining run-out of max. 0.001 mm. Aside from various types of tool holders like collet chucks, hydraulic chucks, milling chucks and tapping holders, their selection encompasses angle heads, measuring devices and cutting tools.

Goal: Minimize forces on thread flanks

In order to further develop their product portfolio, BIG Daishowa is continuously developing new tool concepts in-house at the MEGA Technical Center. One of the products that emerged from these efforts is the MEGA Synchro tapping holder. It is a “compensation chuck,” which uses elastic components to compensate for the synchronization errors between tooling machines and tools. The basic challenge threads pose is to minimize the differences in length arising from the spindle speed as well as the applied feed rate in relation to thread pitch and thread depth, in order to minimize the axial forces that arise on the thread flanks. High axial forces can have a negative impact on the thread flanks and result in decreased lifetime of the tap holder: “Although modern CNC machines are equipped with synchronous spindles, minor synchronization errors still occur,” says Masayuki Doi, development manager at BIG Daishowa. Even minor deviations immediately create high axial forces on the flanks of the tap holder.

Optimized construction thanks to cutting force measuring

In order to optimize the design of the MEGA Synchro, BIG Daishowa relied on a 3-component dynamometer from Kistler. The piezoelectric cutting force measuring device measures a compact 170×140 mm and can be mounted onto the machine tool table. It is exceptionally rigid and accordingly has a high natural frequency, which allows highly precise measurement of forces per cut even at high rotation speeds. “Due to the precise measurements obtained using Kistler’s dynamometer and the conclusions drawn from those, we have been able to tailor the design to such an extent that the forces on the thread flanks have been drastically reduced,” Doi states. In concrete terms: For tapping with a collet chuck, axial forces exert up to 750 N on the tap. Whereas when it comes to MEGA Synchro this is at max. 60 N. This increases the lifetime of an M12 tap by a factor of 2.4.

Due to the precise measurements obtained using Kistler’s dynamometer and the conclusions drawn from those, we have been able to tailor the design to such an extent that the forces on the thread flanks have been drastically reduced.”

Masayuki Doi, development manager at BIG Daishowa

 

Doi is self-assured: “Without Kistler’s cutting force measuring device, we would not have been able to develop the MEGA Synchro.” BIG Daishowa has developed unique collets and nuts for their new tapping holder. In contrast to many other tooling manufacturers, BIG isn't using conventional ER collets but their proper slim collets to clamp the tap. This has a positive effect on the runout accuracy. Moreover, their slim diameter nut is avoiding interference with the work piece.

8/14/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
7/20/2018
Enhanced safety for patients thanks to process monitoring during injection molding
7/16/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
4/11/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
11/14/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
8/11/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
1/4/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
12/22/2016
Kistler makes progress in vehicle development possible
12/22/2016
Kistler Sensor Correvit® SFII measures world record
12/20/2016
Kistler sensors deliver a maximum in data quality under any conditions.
11/7/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
10/5/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
8/17/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2/19/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
11/4/2015
Piezoelectric Measurements with CompactRIO™
6/15/2015
Measurement Solutions for Automotive Test Systems
5/8/2015
Quality Assurance in the Automotive Industry
3/2/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
12/2/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
12/2/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
8/23/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
2/15/2011
End-to-end process monitoring for critical medical moldings
2/7/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
Contact