China’s largest engine manufacturer opts for servo presses from Kistler

Yuchai, the machinery group based in southern China, opts for the NCFN and NCFT servo presses (electromechanical joining systems) from Kistler to manufacture components for engines that comply with the China VI standard. Thanks in part to custom-designed press-fit solutions, Yuchai achieves high product quality, energy efficiency and process transparency.

China's latest exhaust emission standard for commercial vehicles shows that the country is taking a very serious approach to protecting the environment – in spite of the pandemic. "China VI", which is based on Euro VI in many respects, is being introduced in two stages: the VI-a standard already came into force on 1 July 2020, and the strict VI-b norm will apply from 1 July 2023 onwards – with some drastic goals for reductions of CO2, particulate matter (PM) and oxides of nitrogen (NOx) in the mid double-digit percentage range. Over the long term, this should significantly reduce air pollution due to exhaust gases, especially in the nation's mega-cities. But how will these requirements impact automobile manufacturers and suppliers to the automotive industry? There will certainly be major changes to the way vehicles are designed, manufactured and operated.

Guangxi Yuchai Machinery Co., Ltd. (GYMCL or Yuchai for short), has its headquarters at Yulin in the Guangxi Zhuang Autonomous Region (southern China). Yuchai numbers among those automobile manufacturers who foresaw the transformation at an early stage. Founded in 1951, this corporate group has seven other plants throughout China where it produces engines for trucks, buses and other commercial vehicles. With over 15,000 employees, Yuchai posts annual sales of RMB 40 billion (more than EUR 5 billion). As one of China's market and technology leaders for combustion engines, GYMCL embraces cutting-edge technologies and collaborates with universities across the globe including Brunel University in London, RWTH Aachen University in Germany, and Shanghai Jiao Tong University.

Focusing on product quality and resource efficiency

Back in 2016, the foundation stone was laid at Yuchai's Yulin site for two new production halls geared to manufacturing exceptionally resource-efficient, low-emission diesel engines. From day one, servo presses from Kistler were deployed at the relevant stations for the press-fit processes – a choice based on their combination of accuracy, energy efficiency and real-time process monitoring. On 8 January 2018, Yuchai became the first manufacturer in the country to produce China VI-compliant engines with the low emission levels required by the standard – and in 2019, the production line in the second hall also went into operation.

This new manufacturing environment features state-of-the-art production lines. As Head of Operational Safety, Mr. Liu is responsible for technical equipment, maintenance and troubleshooting in the plant. He explains how things have changed:

We used to operate hydraulic and pneumatic press-fit systems. They function well, but they are energy-intensive – and above all, they are very noisy. Thanks to Kistler, we were able to opt for a better alternative – now, everything is much cleaner and quieter, and the whole process is far more orderly."

Mr. Liu, Head of Operational Safety at Yuchai

 

This is an enclosed production environment equipped with large numbers of air conditioning systems, so limiting the noise level is a critical factor. The new approach also yields benefits in terms of setting up the individual stations, and for maintenance: "The systems from Kistler are more compact and more flexible, and they are simpler to commission – so regular maintenance jobs are easier as well,” Liu continues

Force-displacement monitoring – with customized design

Large numbers of NCFN and NCFH series modules from Kistler are deployed for joining processes at many different stations in both of Yuchai's new production halls. Servo presses are used to assemble components such as steel balls, valve seats and guides, seals as well as intake und exhaust manifolds. Production of engine components with press-fitted parts is now placed on an entirely new basis: integrated sensor-based force-displacement monitoring supplies two mutually independent indicators – force and displacement – to allow an accurate assessment of the press-fit process and the mechanisms of the components involved.

As Liu points out: "One simple test is sometimes not enough to detect potential defects and optimize the quality of the process. Thanks to systems from Kistler, we can now respond to challenges that may arise in many areas: part tolerances, machine instability, process errors, and other hidden factors that negatively impact process reliability. This means we can achieve – and maintain – very high quality in our press-fit processes."

As well as the advantages already mentioned, Yuchai also benefits from a customized solution developed by Kistler – in the form of a unique joining module that is not available to any other Chinese engine manufacturer at present. This is an individual variant of the NCFN servo press featuring a very long stroke: 1,000 mm as compared to the standard length of 400 mm (see the box). Liu's final comment: "Thanks to this tailor-made solution, we've been able to sustainably optimize our production. Kistler has demonstrated outstanding flexibility and technical understanding throughout the process. Systems from Kistler are simple to operate, and they're highly reliable – so there's virtually nothing to complain about!"

4/11/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
1/14/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
11/18/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
10/12/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
9/14/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
9/9/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
9/3/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
7/2/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
6/22/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
6/2/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
4/26/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
4/13/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
3/22/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2/8/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
10/5/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
9/18/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
8/20/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
7/22/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
6/9/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
11/15/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
10/23/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
8/15/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
7/17/2019
Turkey opts for weight enforcement with WIM technology from Kistler
6/24/2019
For the next manned flight to the moon: safety that can be measured
6/20/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
5/14/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
4/18/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
4/2/2019
NFL's Jaguars boost their fitness levels with Kistler.
3/25/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
3/18/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
12/17/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
11/27/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
10/8/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
8/31/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
8/14/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
7/16/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
4/11/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
11/14/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
8/11/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
1/4/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
12/22/2016
Kistler makes progress in vehicle development possible
12/22/2016
Kistler Sensor Correvit® SFII measures world record
12/20/2016
Kistler sensors deliver a maximum in data quality under any conditions.
11/7/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
10/5/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
8/17/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2/19/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
11/4/2015
Piezoelectric Measurements with CompactRIO™
6/15/2015
Measurement Solutions for Automotive Test Systems
5/8/2015
Quality Assurance in the Automotive Industry
3/2/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
12/2/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
12/2/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
8/23/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
2/15/2011
End-to-end process monitoring for critical medical moldings
2/7/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Max 25 MB