In the Pole Position with Precision Sensors from Kistler

Modern motorsport vehicles and drivers operate at the absolute limit. Every bit of potential is drawn from core components, such as motors and chassis. To ensure that all individual parts function properly, access to exact measurement data is essential. The lightweight, compact, and long-lasting Kistler onboard sensors are, therefore, the perfect solution for use in motorsport.

Continuous optimization as a challenge

In modern motorsport, details are decisive for victory or defeat. The conditions are hard and demanding. The cars must meet high standards. To detect possible defects at an early stage and thereby be able to continuously optimize the performance, it is essential that high-precision measurement data be accessible at all times.

High-precision sensors for maximum data quality

Motorsport vehicles are constantly pushed to the limit. In these areas, it is a challenge to achieve reliable measurements. Not only do the sensors need to be extremely durable, they must also measure with high precision in the extreme range and, at the same time, be small enough to be installed in restricted spaces. Only in this way is it possible to achieve maximum data quality at all times and under all external influences.

Best performance with Kistler technology

Kistler offers innovative solutions for these application areas. With the durable, high-precision, and space-saving onboard sensors, problems can be detected early on and the motor performance thereby maximized. At the same time, monitoring systems from Kistler ensure continuous control and documentation of the dynamic processes. The sensors and systems supply the race teams with reliable, real-time data that allows them to keep an eye on the performance of the race cars and to make the necessary decisions that can be the difference between victory and defeat. This ensures that the race teams themselves can further optimize race performance at the highest level. You can find more information at our Motorsport pages.

Our highly qualified employees push the limits of what is possible and deliver answers with our customers – and for our customers – to the great questions posed by a connected world around the megatrends mobility, emission reduction, quality control and lightweight construction.
Do you want to play a part in shaping the future? If so, become part of our team.

8/31/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
8/14/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
7/20/2018
Enhanced safety for patients thanks to process monitoring during injection molding
7/16/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
4/11/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
11/14/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
8/11/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
1/4/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
12/22/2016
Kistler makes progress in vehicle development possible
12/22/2016
Kistler Sensor Correvit® SFII measures world record
12/20/2016
Kistler sensors deliver a maximum in data quality under any conditions.
11/7/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
10/5/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
8/17/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2/19/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
11/4/2015
Piezoelectric Measurements with CompactRIO™
6/15/2015
Measurement Solutions for Automotive Test Systems
5/8/2015
Quality Assurance in the Automotive Industry
3/2/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
12/2/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
12/2/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
8/23/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
2/15/2011
End-to-end process monitoring for critical medical moldings
2/7/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contact
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
Contact
(max 25 Mb)