Maximum sensitivity during live production

Turn, press or tilt: vehicle interiors are turning into multifunctional control centers as onboard electronics become more commonplace – and that makes driving safer and more comfortable. But before operating controls for the handbrake, GPS, air conditioning and all the other systems can be integrated into the console, they must undergo precision testing by highly accurate sensors. Their main purpose is to test functionality, but they also check whether the controls give drivers the correct sensory response.

A trend that began decades ago with the first power-assisted window lifters has since become the established standard: onboard electrical systems have replaced mechanical equipment in cars to make driving safer as well as easier. Not so long ago, the driver had to jerk and tug on a clunky lever to apply the handbrake – but now, an elegant push of a button is all it takes. And thanks to multifunctional operating controls such as the rotary knob in the middle of the center console, drivers can intuitively access systems such as the GPS, music or air conditioning without having to take their eyes off the road.

These controls must undergo intensive testing to ensure that they work reliably. They are only installed in a vehicle once test systems have proven that they function correctly. At the heart of the test systems are piezoelectric sensors from Kistler, the measurement technology expert: they measure parameters such as the force exerted on a knob or the detent torque of a rotary adjuster. Thanks to their extremely high sensitivity, these sensors deliver reliable results even when very small physical parameters need to be measured. Any values found to be outside of the defined range for the parameters indicate that manufacturing defects or material faults may be present. Testing avoids the costly procedure of dismantling a switch after it has been installed and – in the worst-case scenario – an operating malfunction that could put life at risk.

Functionality and haptics: two key safety factors

Standard parameters apply not only to the safety-related and functional characteristics of a switch, but also to its haptic attributes. Vehicle drivers expect the operating controls to give them feedback that they can hear and feel – for example, to reassure them that their car is parked safely so it cannot roll away. And pressing a button can communicate even more information to the driver: buttons to operate power windows offer less resistance than controls for functions that are much more critical for safety, such as the handbrake. These different levels of resistance correspond to the operator's natural sensory perception. But in purely technical terms, there is actually no need for such differences.

In these various ways, the tiny measurement sensors deliver multiple benefits for vehicle manufacturers: by ensuring that function tests are precise, they guarantee vehicle safety – and they also help vehicle users to experience the "feelgood factor" as they drive. In short: piezoelectric sensors from Kistler play an essential part in the continuing evolution of onboard automotive electronics.

You might be interested also in:

Solutions from Kistler:
Singling out potentially overloaded vehicles is now a thing of the past. Today, these traffic offenders can be identified using automatic cameras.
“Everyone makes mistakes” – except in the field of medical technology. In the worst-case scenario, defects in the production of insulin pens could put patients’ safety at risk.
Stunned pigs, self-experimentation with showers of glass splinters – these were just some of the ways that vehicles were crash-tested in the first half of the 20th century. Today, crash testing involves high-tech crash dummies.
Preventing ligament tears with advanced technology: tailoring training and physiotherapy precisely to the athlete or patient using highly sophisticated measurement technology is becoming increasingly popular.
Turn, press or tilt: control elements such as hand brakes are put to the test before being installed in vehicles.
If the fasteners that secure the swiveling arm of a crane were to fail, people could be injured – or even lose their lives. Our inspection systems make sure that this could never happen.
Space is the environment that presents the most challenging possible conditions for technical equipment. In order for spacecraft to withstand these extremes and safely transport their crews, our sensors guarantee reliability before the launch.
Contact
Max 25 MB