Programmable sequence control for integrated quality assurance

Shanghai, February 10, 2015 – At this year's SIAF from March 9-11, 2015 in Guangzhou, Kistler will be presenting the latest innovations to its maXYmos product family, which is used to visualize and evaluate production processes. The highlight at Kistler's stand (Hall 5.2, Booth No. C01) is the maXYmos BL 2.2 for manual presses, visitors to the exhibition will be able to see live demonstrations. Kistler is also showing a new update to the maXYmos TL as well as its most recent addition to this product series, the maXYmos NC.

Quality assurance for manually operated processes
The maXYmos BL force-displacement measurement system helps manufacturers attain zero-defect production in their hand-operated press processes. Based on the course of force and displacement measurement curves, the process can be visualized and the quality of the press process evaluated. Deviations are detected immediately and faulty parts can be separated at an early stage. This enables the quality of hand-operated press processes to be reproduced – independently of the respective operating personnel. The result is 100% quality control.
Visitors to SIAF are especially invited to experience the sequencer mode of the maXYmos BL. This mode enables users to define an individual sequence of steps for each press process via the intuitive user interface of the touch display. 11 digital inputs and 8 corresponding outputs can be programmed in order to query and output processrelevant statuses. Up to 128 sequence elements can be configured for each measurement program. The maXYmos BL progressively checks whether all conditions have been fulfilled. In this manner, not only the production process can be controlled and good and bad end results detected, but it can also be deducted whether the desired quality has been attained in each step of the sequence. This can subsequently be reflected graphically. Ultimately, the required quality is ensured without the need for complex external control systems (PLC). In order to update existing manual presses, the measurement system – including sequencer mode – is also available as a retrofit package.

Complete spectrum of force-displacement measurement systems from a single source
Alongside the maXYmos BL, Kistler will also be presenting new functions of its top level system in Stuttgart. The maXYmos TL 1.1.4 includes an extensible language package, which now also encompasses Japanese, Portuguese and Czech. In addition, the system offers faster back-up functionalities, for example via USB or with the related maXYmos computer software. New cable solutions have also been developed to allow the connection of torque sensors.

"With the maXYmos product family, we have set industrial standards in terms of process optimization and quality assurance," says Jens Hoeppner, Product Manager at Kistler. "Our customers enjoy working with these systems and do so very successfully. Thanks to the further development of the underlying technologies they now benefit even more from our expertise and do not even have to get used to a new product."

The series has been completed with the maXYmos NC, which enables control and monitoring of electro-mechanical joining systems. Now, XY sequences for joining and press-fitting processes in combination with NC joining modules can be evaluated and documented and the quality of each individual production step, component or even the entire product can be controlled. This means that optimum cycle times can be implemented with maximum repeat accuracy. In this way, unplanned downtimes are minimized and machine availability is increased, thus improving the productivity of the manufacturing process.

From March 9-11, 2015 visitors to SIAF will be shown Kistler's innovative products and be advised as to how the maXYmos series can be used individually in their own companies at stand C01 in hall 5.2.

Press Release

Captions
Image 1: The uniform philosophy of the maXYmos product family provides user-friendly and intuitive operation. It supports simple and quick start-up of the electro-mechanical NC joining systems.
Figure 2: The Sequencer Mode in the maXYmos BL allows programming of sequence controls, which are used to control the processes. An independent sequence can be created for each measurement program.
Figure 3: Force-displacement measurement system with piezoelectric force sensor for manually operated presses.

15.02.2017
Entdecken Sie im aktuellen Kistler View, welchen Beitrag Kistler zu den grossen Herausforderungen unserer Zeit...
11.11.2016
Mit Kistler MARS Version 3.0 präsentiert Kistler ein umfassendes Update der proprietären Mess-, Analyse- und...
14.10.2016
In der weltweit vernetzten Wirtschaft werden zuverlässige Messlösungen immer wichtiger.
07.06.2016
Entdecken Sie unser aktuelles Kistler News online.
03.05.2016
Das aktuelle Kistler News ist ab sofort online – jetzt reinblättern.
01.02.2016
Entdecken Sie im aktuellen Kistler View, was uns dieses Jahr bewegt.
04.12.2015
Kistler Japan Celebrates its 30th Anniversary and Thanks Its Loyal Customers.
16.10.2015
Fügemodul NCFR von Kistler an der Motek für beste Handhabung und Montage ausgezeichnet.
22.09.2015
Das aktuelle Kistler News ist ab sofort online – jetzt reinblättern.
03.09.2015
Jetzt KiBox Cockpit V2.1 herunterladen und neue Features entdecken.
20.08.2015
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
29.06.2015
Kistler Automotive GmbH als eines der innovativsten Unternehmen Deutschlands ausgezeichnet.
26.06.2015
Die Software für Kistler Kraftmessplatten bietet zahlreiche Neuerungen für die Leistungsdiagnostik in Sport...
22.04.2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data...
23.03.2015
Kistler ist Entwicklungspartner für OEM und bleibt am Puls von Industrie 4.0
13.02.2015
At SIAF 2015 Kistler will be presenting advanced versions of its proven maXYmos product family
10.11.2014
Neuentwicklungen für dynamische Messtechnik am Messestand von Kistler auf der SPS IPC Drives 2014
14.10.2014
Vielfältige Optionen zur Optimierung der Qualitätssicherung durch die Dokumentation und Auswertung von...
29.09.2014
Users obtain a full range of force–displacement measurement systems from one source
03.06.2014
Erweiterung der maXYmos Gerätefamilie zur Steuerung und Überwachung von Produktionsprozessen und...
27.05.2014
Kistler präsentiert an der Sensor + Test 2014 neben bewährter Sensortechnologie viele Neuigkeiten aus dem...
19.05.2014
Anwender erhalten komplette Bandbreite der Kraft-Weg-Messsysteme aus einer Hand
06.02.2014
Die Kistler Gruppe hat 2013 einen Umsatz von 285 Mio. CHF erzielt und ist damit gegenüber Vorjahr leicht...
14.01.2014
Winterthur, 14. Januar 2014 – Dr.-Ing. Oliver Schnerr, Vertriebsleiter der Division Industrial Process Control...
11.11.2013
Vom flexiblen Drehmomentsensor bis hin zum kompletten Prüfstandssystem für hocheffiziente elektrische Antriebe
16.09.2013
Düsseldorf, 3. Juli 2013 - Kistler bietet jetzt auch seine Miniatur-Werkzeuginnen-drucksensoren mit...
13.08.2013
Überwachung, Steuerung und Regelung von RTM- und SMC-Verfahren
24.07.2013
Neuer Längsmessdübel zur berührungslosen Werkzeuginnendruckmessung
08.04.2013
Hightech-Sensorik für extreme Aufgaben auf der SENSOR+TEST 2013
20.03.2013
Die Kistler Gruppe hat 2012 mit einem Rekordumsatz von 279 Mio. CHF resp. mit 19 % Umsatzwachstum ein...
19.03.2013
Die Kistler Gruppe, ein weltweit führender Anbieter von Sensoren zur Messung von Druck, Kraft, Drehmoment und...
15.11.2012
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
08.10.2012
Mit verbesserter Funktionalität und neuen Features wartet die aktuelle Firmware V2.4 für das...
08.10.2012
Kistler präsentiert auf der Fachmesse Fakuma in Friedrichshafen (16. bis 20. Oktober 2012) am Stand 3104 in...
08.10.2012
Kistler präsentiert auf der Fachmesse Fakuma in Friedrichshafen (16. bis 20. Oktober 2012) am Stand 3104 in...
10.09.2012
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
29.06.2012
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
08.05.2012
Kistler präsentiert auf der Fachmesse Automatica in München (22. bis 24. Mai 2012) am Stand 224 in Halle A1...
07.05.2012
Sensoren und Systeme von Kistler überzeugen auch dort, wo Produkte anderer Anbieter an ihre Grenzen stossen....
15.03.2012
Die Organisation CIRP (Collège international pour la recherche productique) wurde 1951 gegründet, um die...
17.02.2012
Auf der MEDTEC Europe vom 13. bis 15. März 2012 in Stuttgart präsentiert Kistler am Stand 4453 in Halle 4, wie...
01.01.2012
Die Kistler Gruppe hat auch 2011 trotz erschwerten Bedingungen mit über 11 % Umsatzwachstum ein solides...
02.11.2011
Der neue Drehmoment-Messflansch KiTorq System von Kistler verschafft Prüfstandsbetreibern durch die bauliche...
02.11.2011
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (22. bis 24. November 2011) am Stand 4A-451...
20.10.2011
Kistler stellt auf der Fakuma eine Online-Prognose für die Formteilqualität beim Spritzgiessen vor: Das neue...
19.10.2011
Kistler bringt den qualitätsorientierten Spritzgiesser der Null-Fehler-Produktion wieder einen grossen Schritt...
28.09.2011
Kistler erweitert seine elektromechanischen NC-Fügemodule NCFB Typ 2160A… mit besonders günstigem...
28.09.2011
Die kabellose telemetrische Übertragung des Kraftsignals und die standardmässige Tauglichkeit für den...
28.09.2011
Der sehr vielseitige und kompakte Monitor mit unschlagbarem Preis-Leistungs-Verhältnis erhält ab der Fachmesse...
03.02.2011
Die Winterthurer Kistler Gruppe blickt auf ein erfolgreiches Geschäftsjahr 2010 zurück. Der Umsatz konnte um...
10.12.2010
Kistler als weltweiter Anbieter von Präzisionssensoren, -systemen und -instrumenten für die dynamische Messung...
24.11.2010
Diese Serie vom Typ 8315A... mit der von Kistler entwickelten K-Beam-Technologie dient zum Messen von...
10.11.2010
Kistlers neue Generation PiezoBeam® Beschleunigungssensoren Typ 8688A(x) bietet bei kleinster Bauart höchste...
29.10.2010
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
10.09.2010
Der neue Druckkraftsensor Typ 9393A… erweitert die erfolgreiche Sensorbaureihe Press Force Sensoren auf einen...
06.09.2010
Mit dem neuen Druck-Temperatur-Kombisensor Typ 6188A… setzt Kistler einen weiteren Meilenstein der...
21.07.2010
Zur Datenerfassung in Laborapplikationen bei Forschung und Entwicklung hat Kistler sein neues...
09.07.2010
Am Produktionsstandort Lorch hat Kistler eine weitere Kalibriereinrichtung für Drehmomentsensoren in Betrieb...
08.06.2010
Als Entwicklungspartner der Automobilindustrie verfolgt die Kistler Gruppe das Ziel, den Fahrzeugherstellern...
19.04.2010
Die Kistler Gruppe hat den Zuschlag für die Instrumentierung von drei Crash-Zentren für die indische...
07.04.2010
Im Rahmen der Optimierung von innermotorischen Vorgängen wird die wirklichkeitsgetreue Abbildung realer...
13.01.2010
Mit dem neuen Typ 4520A... Basic Line steht ein kostengünstiger, auf Dehnmessstreifen-Technologie basierender...
10.12.2009
Die bewährten Press Force Sensoren von Kistler basieren auf dem piezoelektrischen Messprinzip.
18.11.2009
Um Fügeprozesse unter sehr engen Platzverhältnissen und bei geringen Abständen zwischen mehreren Fügestationen...
23.10.2009
Die Kistler Gruppe hat mit Wirkung per 22. Oktober 2009 alle Gesellschaftsanteile der KT Automotive GmbH mit...
14.09.2009
Das Prozessüberwachungssystem CoMo Injection Typ 2869B… von Kistler mit der optional integrierten Funktion...
01.07.2009
Um Produkte von Kistler in CAD-Konstruktionen zu integrieren, bietet der Kistler CAD-Download-Service...
30.04.2009
Die Kistler Gruppe hat mit Wirkung per 30. April 2009 alle Gesellschaftsanteile der Corrsys-Datron...
09.03.2009
Am 5. März fand in Dresden, Deutschland, der Rollout der weltweit ersten Messstrassenbahn statt.
15.01.2009
Die Kistler Gruppe hat mit Wirkung per 1. Januar 2009 alle Gesellschaftsanteile der MSC Automotive GmbH mit...