Kistler Breaks New Ground with Custom Monitoring System for Injection Molding

Orlando, FL. May 7, 2018 – At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding. Unlike ever before, system users can assemble their own package from the vast range of functions available in the system.

ComoNeo is the system of choice for plastics processing companies looking to boost product quality and cost efficiency by optimizing their injection molding processes. Kistler is constantly developing this process monitoring system – not only to accommodate new application cases but also to ensure comprehensive optimization in every respect coupled with maximum cost efficiency.

Based on the measurement of cavity pressure with tried-and-tested sensors from Kistler, users are provided with modular functions to support predictive control of the injection molding process leading to optimum results. Support, monitoring, control and prediction make Version 2.1.0 of Kistler's ComoNeo the leader in process transparency, which is essential for Industry 4.0.

ComoNeo: guiding users to desired results

A key benefit of this system is its ability to support users according to their individual levels of know-how. Kistler has integrated a practical prediction tool into ComoNeo: the Stasa QC software, which uses measured values and statistical analyses to calculate the quality of the manufactured components in advance, and to assess them within the tolerance bands. This special type of process monitoring is particularly useful for manufacturers of high-grade parts – in medical technology or other sectors where safety is critical, for instance.

To ensure optimal product quality and cost efficiency for their injection molding processes, customers can tailor their own ComoNeo with these functions:

  • ComoNeoPREDICT Allows model-based prediction of specified part quality based on the cavity pressure and temperature profiles – for optimum process parameters and transparent processes.
  • ComoNeoMERGE When multiple materials are used, process technology becomes more complex – but ComoNeo 2.1.0 can easily accommodate this challenge. The system monitors and evaluates up to four components with different mold technologies.
  • ComoNeoMULTIFLOW For molds with multiple cavities, this option allows hot runner balancing through individual adjustment of the nozzle temperature – to ensure identical injection conditions in all cavities and automatic correction of deviations.
  • ComoNeoSWITCH This function ensures automated switchover from the injection phase to the holding phase at the ideal time – for balanced injection behavior and optimum mold protection during the process.
  • ComoNeoCOMPOSITE Another new feature: injection molding with the RTM process can now be optimized. Special RTM sensors from Kistler create the conditions for controlled high-quality machining of long-fiber composites.
  • ComoNeoGUARD This function helps users to define monitoring windows that enable accurate separation of good and bad parts on a step-by-step basis. The benefits: guaranteed part quality and less pseudo scrap.
  • ComoNeoRECOVER This feature makes it possible to reproduce a proven injection molding process on a different machine. The user is guided through the adaptation step by step, deviations are identified and the assistant suggests corrective actions.

ComoDataCenter: transparent processes enhance quality and cut costs

As soon as ComoNeo has been specifically tailored to your individual application, everything quite literally comes together in the ComoDataCenter, a database that stores all the process data and establishes a seamless communication with overarching systems. Users benefit from the comprehensive overview of their entire injection molding production, which ultimately provides for a sound basis for ongoing analysis and optimization.

We're offering companies a complete modular and multifunctional package that fulfills all the requirements for intelligent and efficient injection molding. ComoNeo is Industry 4.0 put into practice. Mastery of new processes and greater levels of complexity shows the full extent of what injection molding can achieve in terms of quality – and the potential of process-integrated quality monitoring is far from being exhausted. Development is certainly set to continue."

Dr. Robert Vaculik, Head of Kistler's Strategic Business Field Plastics.

 

Kistler looks forward to welcoming you at NPE in Orlando from May 7 to 11, 2018. Visit Kistler at booth W7145. For more information and to watch a video on ComoNeo, go to: www.kistler.com/comoneo

Mediakit

Mediapaket mit PDF, Worddokument und High-res-Bildern: Kistler Mediakit.zip

03.07.2020
Kistler bringt den neuen Zylinderdrucksensor 66351A für die maritime und stationäre Großmotorenüberwachung auf den Markt.
18.06.2020
Crashtest-Dummies sind aus Fahrzeugentwicklung nicht wegzudenken. Verbesserte Sensortechnik treibt Fahrsicherheit voran
17.06.2020
Neue industrielle Lösung für die Bereiche Automomotive, Medizin-, Halbleiter- und Elektrotechnik.
02.06.2020
Mit dem Datenerfassungssystem KiDAU und der Spezialbatterie KiBAT werden Messungen bei Crashtest effizient und erfolgreich.
26.05.2020
maXYmos TL ML – das weltweit erste Prozessüberwachungssystem, das die strengen FDA- und MDR-Richtlinien erfüllt
18.05.2020
Kistler has entered a cooperation with Vehico. Sensor technologies and driving robots will now be available from a single source.
14.05.2020
Kistler bringt einen neuen uniaxialen Beschleunigungssensor zur Vibrationsüberwachung bei extrem hohen Temperaturen auf den Markt.
21.04.2020
Statt überladene Lastkraftwagen einzeln aus dem Verkehr zu ziehen, könnte eine neue Technologie zu schwere LKW per Blitzer ahnden.
15.04.2020
Der Miniatur-Ladungsverstärker mit IO-Link von Kistler ist für eine Vielzahl von Anwendungen für die Industrie 4.0. geeignet.
26.03.2020
Die Ausbreitung des Coronavirus stellt auch für die Kistler Gruppe eine große Herausforderung dar. Informationen zu der aktuellen Entwicklung.
02.03.2020
Keine optimal funktionierende Gesamtlösung ohne geschulte Mitarbeiter.
26.02.2020
Auf der Intertraffic stellt Kistler sein neues Weigh in Motion System KiTraffic Digital der Öffentlichkeit vor.
10.02.2020
2019 verzeichnete Kistler mit über 2.200 Mitarbeitern einen Umsatz von 466 Millionen Schweizer Franken.
07.02.2020
Intelligent solutions to improve quality and save costs in medical manufacturing.
07.01.2020
An unprecedented measuring range from -500N to 500N marks a major step in improving quality of satellite imaging.
02.12.2019
Dank seiner großen Genauigkeit und Robustheit ermöglicht es KiTraffic Digital, überladene Fahrzeuge direkt zu "blitzen".
18.11.2019
Das Hochgeschwindigkeitskamerasystem HIS von Kistler ermöglicht die optische Analyse von Verbrennungsprozessen in Motoren.
31.10.2019
Auf der SPS 2019 zeigt Kistler ressourceneffiziente Systeme zur Prozessüberwachung mit erweiterter Konnektivität auch am Roboter
25.10.2019
Auf der Blechexpo in Stuttgart zeigt Kistler automatisierte Prüfsysteme zur Qualitätssicherung für Serienteile und Umformprozesse
22.10.2019
Innovative measurement chain to advance development and validation processes of state-of-the-art vehicles
21.10.2019
Wie lässt sich der Antriebsstrang eines Plug-in-Hybrid-Fahrzeugs optimieren? Kistler forscht dazu gemeinsam mit der Uni Bath (UK).
16.10.2019
Höchste Präzision, Einheitsempfindlichkeit und höhere Robustheit: Zur K 2019 zeigen wir innovative Werkzeuginnendrucksensoren
07.10.2019
Das Leistungsdiagnosesystem Quattro Jump ermittelt Leistungsparameter und hilft so Verletzungen an Gelenken vorzubeugen
30.09.2019
Dank neuer modellbasierter Klopferkennungsmethoden liefert die KiBox KID dem Anwender wertvolle Zusatzinformationen.
30.09.2019
Der Kistler Standort Sindelfingen wurde im Sommer 2019 für sein wirksames Umweltmanagement nach DIN EN ISO 14001 zertifiziert.
27.09.2019
The Czech government has approved Weigh In Motion with KiTraffic for direct law enforcement of overloaded trucks.
19.09.2019
Die Kistler Gruppe erweitert drei Standorte in der Schweiz und in Deutschland und setzt in bewegten Zeiten ein starkes Zeichen.
17.09.2019
An der außerordentlichen Hauptversammlung am 16. September 2019 wurden neue zwei neue Verwaltungsratsmitglieder ernannt.
10.09.2019
Wir haben die Schweizer Nachwuchsingenieure erfolgreich mit einem S-Motion Sensor inklusive Beratung und Service unterstützt.
06.09.2019
Auf der Messe für Kunststoffverarbeitung K2019 zeigt Kistler innovative Lösungen und Produkte zur intelligenten Prozessüberwachung.
26.08.2019
Auf der Motek 2019 zeigt Kistler ressourceneffiziente und digital vernetzte Systeme für die industrielle Fertigung und Montage.
21.08.2019
Warum Forscher zur Verbesserung des Tsunami-Schutzes Kraftsensoren von Kistler einsetzen
16.08.2019
Warum die Belegschaft von Kistler für krebskranke Kinder spendete
22.05.2019
Kistler präsentiert auf der Sensor + Test 2019 erweitertes Portfolio zu Messtechnik und Datenanalyse.
24.04.2019
Zuverlässige Prozessüberwachung in der Fertigung von Medizinprodukten – von der Versuchsplanung bis zur Serienproduktion.
08.04.2019
Weltneuheit: Mit KiXact von Kistler bekommen Sie Messunsicherheiten in den Griff.
08.04.2019
Kistler zeigt auf der Control 2019 erweitertes Produktportfolio Testautomation zur Qualitätssicherung bei großen Stückzahlen.
05.04.2019
Einzigartige DTI-Technologie von Kistler Zukunftsfähige Lösungen zur Verbesserung von Fahrdynamik- und Betriebsfestigkeitsstests
21.03.2019
Gewicht, nicht Anzahl der Fahrzeuge, belastet die Infrastruktur: Steigende Achslasten mit Weigh In Motion Systemen im Blick behalt
20.03.2019
Alles aus einer Hand: Kistler komplettiert Messkette für Fahrzeugentwicklung.
15.03.2019
Valentin Vogt wurde zum neuen Verwaltungsratspräsidenten der Kistler Gruppe gewählt.
14.03.2019
Der langjährige Kunde von Kistler hat bereits über 4000 Lineas WIM Sensoren installiert.
20.02.2019
Serving customers’ growing demands: the Kistler Group opens its first official sales center in Canada
18.02.2019
Die Kistler Gruppe zeigt auf der Fachmesse Fastener Fair 2019 in Stuttgart vom 19. bis 21. März am Stand 862, Halle 1 ihre Prüf- und Analysesysteme für Schraubverbindungen..
11.02.2019
Weltweit größter Piezo-Kraftsensor misst bis 450kN
06.02.2019
Neues Qualitätsniveau: Kistler und NETZSCH demonstrieren, wie sich ihre Systeme zur Verarbeitung von Composites ergänzen.
05.02.2019
Die Kistler Gruppe stärkt ihre Präsenz am chinesischen Markt. Am 5. Februar eröffnete das Unternehmen ein neues Büro in Shanghai.
31.01.2019
Die Zahlen des Geschäftsjahrs 2018 sind Anlass zu feiern: 2020, zum 60. Jubiläum von Kistler, geht es gemeinsam aufs Schiffsreise.
11.12.2018
Große Mengen von Messdaten ("Big Test Data") gezielt und effizient auswerten: AMS bringt noch mehr Digitalkompetenz in die Kistler Gruppe.
28.11.2018
Einbauunempfindlich und präzise: Der neue M8-Sensor Typ 6044A in Anti-Strain-Bauweise liefert zuverlässig hochwertige Ergebnisse.
20.11.2018
Motorsport: Neue Absolutdrucksensoren 4080B/BT von Kistler – für Echtzeitüberwachung mit maximaler Messgenauigkeit und Signalqualität!
16.10.2018
Auf der Fakuma vom 16. bis 20. Oktober 2018 in Friedrichshafen zeigt die Kistler Gruppe das weiterentwickelte Prozessüberwachungssystem ComoNeo für hohe Qualität, Effizienz und Transparenz beim Spritzgießen.
08.10.2018
Seit Kurzem gehört die SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH zur Kistler Gruppe.
24.09.2018
Die Kistler Gruppe erweitert das weltweit umfassendste Produktportfolio an Radkraftmesssystemen um eine weitere Variante: Mit dem neuen RoaDyn S6GT 6-Komponenten- Radkraftmesssystem steht nun ein individuell konfigurierbares, hochpräzises Messrad mit gesteigertem Messbereich für schwere Nutzfahrzeuge und Off-Highway-Maschinen zur Verfügung.
21.09.2018
Vester zeigt auf der Fakuma 2018, was Prüfautomation alles leisten kann
17.09.2018
Spitzenleistungen, Teamspirit und Leidenschaft für die Sache – das verbindet die Tigers Tübingen und die Kistler Gruppe.
10.09.2018
Hochpräzises rotierendes Dynamometer in Kombination mit innovativem Spannzangenfutter verlängert die Standzeit von Werkzeugen und senkt die Fertigungskosten.
06.09.2018
Maschinenbauer LIK wird Teil der Kistler Gruppe und stärkt Marktzugang für Elektrofahrzeuge
28.08.2018
Mehr Transparenz in der Kunststoffverarbeitung
21.08.2018
Die Kistler Gruppe führt mit ihrem Bremskraft-Messsystem Typ 2899A eine kompakte und mobile Messlösung für die effizientere Instandhaltung des Rollmaterials im internationalen Bahnbetrieb ein.
21.08.2018
In Aachen wird ein neues Kompetenzzentrum für Produktionssteuerung und –leitsysteme eröffnet.
31.07.2018
Nähe und kompetenter Service sind für die Kistler Gruppe seit jeher die Hauptbestandteile in der Zusammenarbeit mit seinen Kunden. Um jetzt auch der wachsenden Nachfrage im Norden Deutschlands gerecht zu werden, eröffnen die Messtechnikexperten am 11. September einen weiteren Standort in Wolfsburg.
25.07.2018
Auf ihrem Weg zu Olympia 2020 vertraut sie auf die Kistler Messexpertise.
18.07.2018
Effektive Überwachung per Dehnungssensor schützt Maschinen und Werkzeuge
03.07.2018
Kistler wurde am 29. Juni mit dem begehrten TOP 100-Innovationspreis in der Kategorie Innovationserfolg ausgezeichnet
25.06.2018
Nach knapp zwei Jahren Entwicklungszeit stellt Kistler mit dem MicroDyn das weltweit kleinste in Serie hergestellte Zerspankraftmessgerät vor.
19.06.2018
Kistler führt den weltweit ersten Hochtemperatur-Beschleunigungssensor für den Dauerbetrieb bis 700° C zur sicheren Überwachung von Gasturbinen ein.
11.06.2018
Die Schweizer Messtechnikexperten geben das höchste Investitionsbudget für Forschung und Entwicklung der Firmengeschichte frei.
11.05.2018
Digitalisierung, Internet of Things und Industrie 4.0 stellen uns vor grosse Herausforderungen. In der neusten Ausgabe des Kistler View finden Sie unsere Antworten auf die Fragen von morgen.
09.05.2018
Auf der Sensor + Test 2018 präsentiert Kistler einen wichtigen Meilenstein: das neue Datenerfassungssystem KiDAQ. Mit dem ganzheitlichen System erhalten Anwender eine weltweit einzigartige Transparenz ihrer Messdaten.
08.05.2018
Auf der Stanztec 2018 (19. – 21. Juni in Pforzheim) präsentiert die Kistler Gruppe Sensorik, Mess- und Prüfsysteme für die Stanztechnik.
03.05.2018
Auf der Automatica 2018 in München (19. – 22. Juni 2018) zeigt die Kistler Gruppe vielfältige Möglichkeiten, um mit Sensoren und Prozessüberwachungssystemen die industrielle Fertigung zu unterstützen und Qualitäts- und Effizienzgewinne zu realisieren.
24.04.2018
Auf der Control 2018 zeigt die Kistler Gruppe ihr erweitertes Portfolio an industriellen Prüfsystemen zur Qualitätssicherung.
12.04.2018
Der Weltmarktführer in Messtechnik unterstützt die Leidenschaft für Innovation und Technologie durch eine dreijährige Partnerschaft.
06.03.2018
Auf der Weltleitmesse für Qualitätssicherung Control 2018 zeigt die Kistler Gruppe ihr erweitertes Portfolio an industriellen Prüfsystemen.
16.02.2018
Auf der Intertraffic 2018 stellt die Kistler Gruppe ihre umfassenden KiTraffic Weigh In Motion (WIM) Lösungen vor, die Straßenbesitzer und Straßenverkehrsbehörden bei der Überwachung der Einhaltung von Gewichtsvorschriften und bei gewichtsbasierten Mautsystemen unterstützen.
15.02.2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31.01.2018
Das neue KiSprint stellt Trainern und Athleten ein effizientes Mittel zur Verfügung, um unter wettkampfanalogen Bedingungen den Sprintstart biomechanisch zu optimieren. Die robuste und mobile Lösung verfügt über umfassende Auswertungsmöglichkeiten per Software und kann individuell angepasst und erweitert werden.
24.01.2018
Kistler verzeichnete 2017 ein Wachstum von 18 %. Fokusthema für 2018: die digitale Transformation.
23.01.2018
Overcoming the complexities of RTM – with Kistler
12.10.2017
Auf der SPS IPC Drives 2017 stellt Kistler den weltweit ersten digitalen Ladungsverstärker vor.
09.10.2017
Das Messwerterfassungsgerät Kistler Typ 5074A ist ein Durchbruch in der Ladungsverstärker-Technologie für die industrielle Anwendung
06.10.2017
Ob Hybridantrieb oder Elektrofahrzeug: Wer etwas verändern will, muss messen und verstehen.
27.09.2017
Unsere Experten präsentieren Ihnen Messtechnologien von Kistler für anspruchsvolle Raumfahrtanwendungen.
05.09.2017
Kistler zeigt auf der Fachmesse Fakuma 2017 in Friedrichshafen vom 17. bis 21. Oktober die neuen Funktionen von ComoNeo (Halle A3, Stand 3104)
31.08.2017
Die Kistler Gruppe präsentiert die gesamte Bandbreite ihrer Lösungen zur integrierten Qualitätssicherung
25.08.2017
Kistler übernimmt per heute die Vester Elektronik GmbH (DE), die sich erfolgreich auf die Schwerpunkte Sensorik und Prüfautomation konzentriert hat.
11.08.2017
Mit Hilfe von Kistler Radkraftsystemen erhält der Automobilhersteller nun reale Daten zur exakten Reifenmodellierung.
11.07.2017
Kistler übernimmt die IOS GmbH (DE), Anbieter von Manufacturing Execution Systems (MES).
06.07.2017
Per 5. Juli gehört die in Tettnang ansässige eso GmbH (DE) zur Kistler Gruppe.
20.06.2017
Einbindung in übergeordnete MES-Systeme für perfekt synchronisierte Produktionsdaten.
02.05.2017
Kistler präsentiert neue Messausrüstung für anspruchsvolle Fahrzeugtest-Anwendungen
25.04.2017
Zur Moulding Expo 2017 zeigen wir, wie einfach es ist, die zur Qualitätssicherung erforderliche Messtechnik in Spritzgießwerkzeuge einzubauen.
12.04.2017
Auf der Weltleitmesse für Qualitätssicherung Control zeigt die Kistler Gruppe mobile Prüfsysteme der Marke Schatz.
12.04.2017
Neuer Labor-Ladungsverstärker LabAmp 5167A für die Zerspankraftmessung
11.04.2017
Messausrüstung für anspruchsvolle T&M Anwendungen
01.02.2017
Die Kistler Gruppe wächst stetig und investiert weltweit in hochkarätige Fachkräfte.
17.01.2017
Olympiasieger Anthony Ervin und Kistler schreiben gemeinsam eine Erfolgsgeschichte.
02.12.2016
Mit dem vermutlich grössten Stelleninserat der Schweiz sucht Kistler nach über 40 Spezialisten.
11.11.2016
Mit Kistler MARS Version 3.0 präsentiert Kistler ein umfassendes Update der proprietären Mess-, Analyse- und Auswertungssoftware für Kistler Kraftmessplatten.
21.10.2016
Kistler steigert die Effizienz und Zuverlässigkeit von maritimen und stationären Großmotoren durch die Überwachung und Kontrolle des Verbrennungsprozesses
10.10.2016
Mit dem NCFE-Fügemodul erweitert Kistler sein Portfolio elektromechanischer Fügemodule.
30.09.2016
Die Kistler Gruppe verzeichnet per Ende August 2016 einen Auftragseingang von 233.3 Millionen Schweizer Franken und ist damit gegenüber der Vorjahresperiode um 8.4% resp. währungsbereinigt um 5.6% gewachsen. Mit der Einweihung des neuen Deutschland-Hauptsitzes in Sindelfingen wurde der Grundstein für weiteres Wachstum gelegt. Mit der Übernahme der Schatz-Gruppe erweitert Kistler sein industrielles...
07.09.2016
An der diesjährigen K-Messe vom 19. bis 26. Oktober in Düsseldorf präsentiert Kistler aktuelle Produktneuheiten mit Bezug zu Industrie 4.0.
30.08.2016
An der diesjährigen Motek vom 10. bis 13. Oktober in Stuttgart stellt Kistler die neuen Fügemodule NCFE und NCFR sowie die neuste Generation der maXYmos Monitoringsysteme vor.
12.07.2016
Der Kistler Sensor Typ Correvit® SFII misst den neuen Weltrekord für die schnellste 0-100 km/h.
12.05.2016
Schraubtechnologie ergänzt das industrielle Anwendungsportfolio.
27.04.2016
Nach langer Phase der Planung, Vorbereitung und Umsetzung bezieht die Kistler Instrumente GmbH ihren neuen Deutschland-Hauptsitz auf dem Flugfeld Böblingen/Sindelfingen.
12.02.2016
Kistler Lorch GmbH für herausragende Arbeitgeberqualitäten geehrt
02.02.2016
Kistler wächst auch 2015 und der Ausbau in Deutschland verläuft nach Plan.
28.01.2016
Präzise Radkraftmessungen mit minimalem Konfigurationsaufwand
26.11.2015
Mehr Flexibilität und Zuverlässigkeit bei der Verbrennungsanalyse
02.11.2015
Neuer piezoresistiver Sensor mit Temperaturfühler und integrierter Signalaufbereitung.
27.10.2015
Maximale Flexibilität bei Produktprüfung und -entwicklung mit Kistler
16.10.2015
Kistlers NCFR Fügemodul überzeugt in der Kategorie Handhabung und Montage
05.10.2015
Der Massstab für 100 % Kontrolle bei linearen Fügeprozessen mit rotierendem Anteil
18.09.2015
Kistler Gruppe: nachhaltige Sicherung der Wettbewerbsfähigkeit.
15.09.2015
Schnelle Analyse von Leistung und Kraft mit Kistler MARS 2.1.
03.09.2015
Major-Update für Kistlers mobiles Motorenindiziersystem.
01.09.2015
Neue Massstäbe in der automatisierten Prozessüberwachung beim Spritzgiessen.
25.08.2015
Kistler präsentiert an der Motek 2015 drei aktuelle Produktneuheiten
29.06.2015
Kistler Automotive GmbH als eines der innovativsten Unternehmen Deutschlands ausgezeichnet.
26.06.2015
Kistler mit ASCO-Award Gold für die beste Unternehmenstransformation der Schweiz ausgezeichnet.
26.06.2015
Die Software für Kistler Kraftmessplatten bietet zahlreiche Neuerungen für die Leistungsdiagnostik in Sport und Rehabilitation.
22.04.2015
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
10.11.2014
Neuentwicklungen für dynamische Messtechnik am Messestand von Kistler auf der SPS IPC Drives 2014
14.10.2014
Vielfältige Optionen zur Optimierung der Qualitätssicherung durch die Dokumentation und Auswertung von Produktionsdaten des CoMo Injection Systems
29.09.2014
Users obtain a full range of force–displacement measurement systems from one source
03.06.2014
Erweiterung der maXYmos Gerätefamilie zur Steuerung und Überwachung von Produktionsprozessen und Qualitätssicherung
27.05.2014
Kistler präsentiert an der Sensor + Test 2014 neben bewährter Sensortechnologie viele Neuigkeiten aus dem Bereich der Messelektronik.
19.05.2014
Anwender erhalten komplette Bandbreite der Kraft-Weg-Messsysteme aus einer Hand
06.02.2014
Die Kistler Gruppe hat 2013 einen Umsatz von 285 Mio. CHF erzielt und ist damit gegenüber Vorjahr leicht gewachsen.
11.11.2013
Vom flexiblen Drehmomentsensor bis hin zum kompletten Prüfstandssystem für hocheffiziente elektrische Antriebe
Kontakt
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
Kontakt
(max 25 Mb)