Calibration service – accredited torque calibration from Kistler now available up to 100,000 N·m


温特图尔,2025年9月——作为全球领先的动态测量技术供应商,奇石乐拥有全面的校准服务组合,并在扭矩校准领域树立新标杆: 奇石乐提供DAkkS认证的可追溯校准服务——涵盖第三方产品——测量范围横跨4 mN·m至100,000 N·m全区间,助力各行业企业以最高标准完成测量任务。

Studies show that around eight percent of all calibrated testing and measuring devices are found to have deviations that require adjustment or repair. Undetected measurement errors lead to inaccurate results, increased reject rates and production losses. The management of recurring calibration intervals is therefore an important factor in differentiating oneself from the competition and ensuring consistently high quality in development and production.

Torque calibration is an essential part of quality assurance in numerous industries, from the automotive and aerospace sectors to medical technology. Kistler offers accredited torque calibrations in accordance with ISO 17025 and guarantees minimum measurement uncertainties of up to 0.01 percent. The very wide measuring range from 4 mN·m to 100,000 N·m is covered by five ultra-modern calibration systems. Thanks to the unique calibration system and particularly in the upper measuring range of 5,000 to 100,000 N·m, Kistler can also offer service calibrations for third-party products – providing customers with additional high-quality calibration services from a single source.

Accredited torque calibration is an essential part of quality assurance in many industries.
Torque calibration is an essential part of quality assurance in numerous industries, from the automotive and aviation sectors to medical technology.

Setting individual intervals for torque calibration

测量仪器在全生命周期内会受到多种因素影响:磨损与老化可能导致传感器精度下降;过载与冲击可能造成永久形变或损坏;温度及环境因素可能改变其测量特性。为此,奇石乐建议通过定期校准确保最高测量可靠性。推荐校准间隔为 6 个月至 2 年,具体需根据设备运行条件确定,并可通过个性化风险分析精准制定。

提供一般服务型与可溯源型的扭矩校准

除获得德国认证机构(DAkkS)依据ISO 17025标准认证的校准服务外,奇石乐还提供基于该标准的工厂校准与一般服务校准。定期扭矩校准是优化生产流程、维持高品质标准的关键。通过持续监测测量仪器的计量性能,用户可深入了解其工艺流程,并确定最佳校准周期。

凭借数十年测量技术经验、前沿技术实力及全球认可校准实验室网络,奇石乐已成为行业领先的校准服务供应商,助力全球企业实现高效生产。对于追求最高测量精度与长期工艺稳定性的客户而言,奇石乐卓越的服务质量与专业技术能力可带来切实价值。

Need a consultation?

Our experts are just a click away.

Learn more about