What is cavity pressure?
In injection molding, cavity pressure – the pressure in the interior of the injection mold, which is filled with liquified plastic – is a key indicator of the quality of the molded part that is produced. The cavity pressure profile enables specific observations to be made with respect to optimal process parameters throughout the entire process (that is, during the injection phase, the compression phase and the holding pressure phase). This, in turn, makes it possible to distinguish good parts from bad parts directly on the factory floor.