When Fritz Müller founded Gebrüder Müller Apparatebau GmbH & Co. KG (GEMÜ) in 1964, no one could have foreseen the unique success story that would emerge. Today, with the second generation at the helm, this hidden champion from the northeast of Baden-Württemberg has more than 2,500 employees and is a global market leader in valve, measurement and control technology. In addition to two factories in Germany, GEMÜ also operates production facilities in Brazil, China, France, India, Switzerland and the US. In many sectors, such as medtech and pharmaceuticals, semiconductor production, and the food and beverage industry, control of process media (gases, steams and liquids) is essential.
GEMÜ has had a long tradition of plastics processing ever since Fritz Müller achieved a milestone in valve technology with the first process valve made of plastic (PVC) in 1964. Today, GEMÜ uses over 100 different plastics in various processes to manufacture its comprehensive product portfolio. GEMÜ’s Development department drives innovation and develops customer-specific solutions that comply with the strictest standards – all tool and mold manufacturing takes place in-house. To meet the increasingly strict quality requirements in the field of injection molding, GEMÜ is already using measurement technology and process monitoring systems from Kistler at its locations in Germany, Switzerland and France. The combination of cavity pressure sensors and monitoring and control systems that are directly integrated into the machinery allows for targeted development and optimization of the injection molding process on the basis of case-specific criteria.








![Plastics processing at the highest level  [object Object]](https://kistler.cdn.celum.cloud/SAPCommerce_Document_Preview/961-965e.webp)