ウィンタートゥール、2021年11月 —— 耐食性の締結部品は自動車業界にとって不可欠であるだけでなく、風力タービン業界においても同様に重要な役割を果たしています。そうした中で、ドルケン(Dörken)は、摩擦係数を特定するためのテストスタンドとしてキスラーのANALYSEシステム4台を採用しています。これにより、厳しさを増す試験要件を満たし、特に亜鉛フレークコーティングにおいて世界中の統一規格を確実に遵守できるようになっています。
屋根用の塗料、ニスや積層板が売上(総額約3億ユーロ)の大半を占める化学薬品会社の敷地に、なぜ締結部品の試験ラボがあるのでしょうか?1892年に設立されたエヴァルト・ドルケンAG(Ewald Dörken AG)は、ドイツのヘルデッケ(ノルトライン=ヴェストファーレン州)に本社を構えています。同社の専門技術には、建築物のあらゆる種類の仕上げ材やコーティングのほか、特に締結部品に重点を置いた防食処理加工があります。自動車に使用されている締結部品は、そのほぼすべてにコーティング加工が施されており、たいていはいわゆる亜鉛フレークコーティング加工が用いられています。この技術では、小型の鋼鉄製コンポーネントを洗浄して、コーティング剤の入った恒温槽に浸漬させ、余剰分を落としてから、最終工程で熱を加えます。卑金属である亜鉛は、その犠牲防食作用により、コーティングされた金属を保護します。これと同じプロセスは、風力タービンの大型のM24アンカーボルトにも使用されています。
ただ、このプロセスは、ドルケンの自社拠点で行われるのではなく、コーティングサービスを担う企業が行っています。これらの独立系企業やライセンス取得者は、ドルケンから材料の供給と監査を受けています(一部の企業は各種の締結部品テストスタンドも使用)。その世界的なネットワークには、こうした「コーティング関連企業」が200社以上参加しており、これらの会社によって、自動車業界、風力発電・機械工学分野、さらに数多くの特殊用途向けの締結部品、ナットや他の各種部品に適切な防食処理が施されています。亜鉛フレークコーティングのほか、コイルコーティングやガルバニックコーティングといった技術もありますが、これらの手法は数量から見て、それほど重要とはあまり言えません。







![Excellent protection and reliable processes [object Object]](https://kistler.cdn.celum.cloud/SAPCommerce_Document_Preview/961-575e.webp)