Glossary
Linearity
Symbol Lin Unit %FSO Linearity is defined as the closeness of the calibration curve to a specified line (source: ANSI/ISA-S37.1). Linearity represents the maximum deviation between ideal and actual output signal characteristics in relation to the measurand in a specific measuring range. It is expressed in percentage of the range of measurement signal (full scale output). Note: Quartz crystals produce an electric charge, which is exactly proportional to the load. However, certain unavoidable deviations occur due to the mechanical construction of the sensor.
|
|

Fast access to select products
view

Come visit us at NATMEC Booth #203 Jun 4 - 7. Kistler is a proud sponser of ICWIM6
read more...

Capacitive MEMS, Triaxial Accelerometer, Type 8395A...
read more...

Force Feedback Capacitive Accelerometer, Type 8330B3
read more...
|