Kistler North America




Glossary

All  |  A  |  B  |  C  |  D  |  E  |  F  |  G  |  H  |  I  |  L  |  M  |  N  |  O  |  P  |  Q  |  R  |  S  |  T  |  U  |  V  |  W  |  Z 

Frequency range (Dynamics)

Symbol

f

Unit

Hz

Because of their mechanical quality, piezoelectric sensors have very low damping. The useful frequency range is limited in the upwards direction by the increasing resonance rise.

Symbol:

• f        =      measuring frequency
• fn      =      natural frequency
• A/A0  =      amplitude ratio

The following approximate values apply to the amplitude error or achievable accuracy as a function of frequency:

• accuracy 10 %  ®     fmax » 0,3 · fn
• accuracy   5 %  ®     fmax » 0,2 · fn
• accuracy   1 %  ®     fmax » 0,1 · fn

Schematic presentation of frequency response and phase response

Schematic presentation of frequency response and phase response

Note: In their dynamic behaviour, piezoelectric sensors are superior to all other measuring methods. Their high rigidity results in the highest possible natural frequencies. Piezoelectric sensors are thus ideal for measuring measurands which change rapidly over time. Their dynamic behaviour is thereby largely determined by the surrounding structure. Therefore the frequency response of the entire measuring arrangement must be investigated for the largest possible, useful measuring range.

There are two possibilities here: frequency analysis, f.e. pressure sensors in shock tube or finite-element method.

 
 
Quick Look Product Finder
KIC_S_pfndr
Fast access to select products
view

WIM Show - NATMEC/ICWIM
TRB_logo
Come visit us at NATMEC Booth #203 Jun 4 - 7. Kistler is a proud sponser of ICWIM6
read more...

New Triaxial K-Beam
8395_BG
Capacitive MEMS, Triaxial Accelerometer, Type 8395A...
read more...

Kistler View 2012

New ServoK-Beam
8330B3_BG
Force Feedback Capacitive Accelerometer, Type 8330B3
read more...

PRT Family
Type 4260/62/64A...
PRT Configurator
open...

Kistler Video
Video: Kistler delivers success - worldwide
Kistler Image Video
Play video

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +1 716 691 5100