Manufacturing




Research and Development

The evaluation and analysis of manufacturing methods can be based on different process variables. Cutting, for example, can be examined with the aid of measurands such as acceleration or acoustic emission. Another example is tool life, which is still frequently determined by the involved method of measuring the width of wear marks.

One measurand for evaluating production processes that impresses both researchers and practitioners through its ease of application and considerable predictive power is force.

Evaluating production processes

Mechanical processes generate forces in one or more directions as well as torques. The great strength of Kistler force measurement products is their ability to acquire these variables extremely accurately and responsively, yet largely eliminate measurement error introduced by environmental factors. They therefore provide viable measurement results for process analysis, which is a strenght of Kistler force measurement products. Cutting forces on, for example, a machine tool can only be measured if suitable instruments can be interposed in the direct load path. The wealth of experience and extensive know-how accumulated by Kistler over the past 40 years in this sector are now available to our customers in the form of tried and tested force measurement systems.


» Direct access to the Product Finder, Manufacturing

 
 
Modal show
sem_logo
Come visit us at IMAC booth 601, Jan. 30 – Feb. 2
read more...

Quick Look Product Finder
KIC_S_pfndr
Fast access to select products
view

Expo Manufactura
expoman
Come visit us at booth 1037, Marzo 6 - 8
read more...

New Triaxial K-Beam
8395_BG
Capacitive MEMS, Triaxial Accelerometer, Type 8395A...
data sheets...

CAD Download
Kistler CAD Download Service
Kistler CAD Download Service Brings Sensors and Electronics Straight into Design
more...

PRT Family
Type 4260/62/64A...
PRT Configurator
open...

New ServoK-Beam
8330B3_BG
Force Feedback Capacitive Accelerometer, Type 8330B3
data sheet...

Kistler Video
Video: Kistler delivers success - worldwide
Kistler Image Video
Play video

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +1 716 691 5100