Plastics




Setup and Service

Setup and Service
When setting up and servicing mold cavity pressure sensors the following three steps are important: insulation testing, sensitivity testing and repair of the single-wire cables.


Insulation Testing

Pressure sensors are maintenance-free, however the insulation should be checked during a mold service. The following instructions must be observed:

• Ensure the connector is dry
• When cleaning, cover the mounting bore or keep it clean
• Use cleaning spray Type 1003 
• Check insulation with the tester Type 5493:
  Reference value >1013 Ω


» Troubleshooting


Sensor Sensitivity

An incorrect installation of a sensor affects its sensitivity. The sensitivity of an installed sensor must therefore be tested, if possible before setting up the mold on the machine.

• Test the sensitivity of the sensor with the set Type 5993A...

» Troubleshooting


Repair of Single-Wire Cables

Repair slight damage to the cable with repair kit Type 1207. Solder broken cables and cover joint with Teflon sheath and heat-shrink tubing of the repair kit Type 1207.

» Single-Wire cable repair

 
 
Quick Look Product Finder
KIC_S_pfndr
Fast access to select products
view

QualityMolding
Logo_QualityMolding_Teaser_110.gif
Quality Molding is the 100% quality seal for injection molding processes.
more...

WIM Show - NATMEC/ICWIM
TRB_logo
Come visit us at NATMEC Booth #203 Jun 4 - 7. Kistler is a proud sponser of ICWIM6
read more...

News 29.10.2010
Img_clearpixel
Kistler and STASA develop an automatic method for the prognosis of injection molded part quality
more...

New Triaxial K-Beam
8395_BG
Capacitive MEMS, Triaxial Accelerometer, Type 8395A...
read more...

New ServoK-Beam
8330B3_BG
Force Feedback Capacitive Accelerometer, Type 8330B3
read more...

PRT Family
Type 4260/62/64A...
PRT Configurator
open...

Kistler Video
Video: Kistler delivers success - worldwide
Kistler Image Video
Play video

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +1 716 691 5100