Documented Proof of Quality

Especially with regard to end-to-end traceability of a product and its production process, production documentation plays an ever-more important role. Measurement of cavity pressure means that the most important process information is available for every cycle and every molded part that is produced. Cavity pressure is therefore the ideal solution for documenting production based on actually measured independent values. In addition to the process curve, each molded part has an associated good/bad evaluation. This information can be used to generate quality documents with the aid of the Kistler statistics tool, for instance. This provides the most important production data for the molded part's life cycle.
|
|
|

Fast access to select products
view

Quality Molding is the 100% quality seal for injection molding processes.
more...

Come visit us at NATMEC Booth #203 Jun 4 - 7. Kistler is a proud sponser of ICWIM6
read more...

Kistler and STASA develop an automatic method for the prognosis of injection molded part quality
more...

Capacitive MEMS, Triaxial Accelerometer, Type 8395A...
read more...

Force Feedback Capacitive Accelerometer, Type 8330B3
read more...
|