Kistler Singapore




Glossary

All  |  A  |  B  |  C  |  D  |  E  |  F  |  G  |  H  |  I  |  L  |  M  |  N  |  O  |  P  |  Q  |  R  |  S  |  T  |  U  |  V  |  W  |  Z 

Linearity

Symbol

Lin

Unit

%FSO

Linearity is defined as the closeness of the calibration curve to a specified line (source: ANSI/ISA-S37.1).

Linearity represents the maximum deviation between ideal and actual output signal characteristics in relation to the measurand in a specific measuring range. It is expressed in percentage of the range of measurement signal (full scale output).

Note: Quartz crystals produce an electric charge, which is exactly proportional to the load. However, certain unavoidable deviations occur due to the mechanical construction of the sensor.

 
 
Kistler View 2012

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +65 631 67331