Kistler Italia




Glossary

All  |  A  |  B  |  C  |  D  |  E  |  F  |  G  |  H  |  I  |  L  |  M  |  N  |  O  |  P  |  Q  |  R  |  S  |  T  |  U  |  V  |  W  |  Z 

Frequency range (Dynamics)

Symbol

f

Unit

Hz

Because of their mechanical quality, piezoelectric sensors have very low damping. The useful frequency range is limited in the upwards direction by the increasing resonance rise.

Symbol:

• f        =      measuring frequency
• fn      =      natural frequency
• A/A0  =      amplitude ratio

The following approximate values apply to the amplitude error or achievable accuracy as a function of frequency:

• accuracy 10 %  ®     fmax » 0,3 · fn
• accuracy   5 %  ®     fmax » 0,2 · fn
• accuracy   1 %  ®     fmax » 0,1 · fn

Schematic presentation of frequency response and phase response

Schematic presentation of frequency response and phase response

Note: In their dynamic behaviour, piezoelectric sensors are superior to all other measuring methods. Their high rigidity results in the highest possible natural frequencies. Piezoelectric sensors are thus ideal for measuring measurands which change rapidly over time. Their dynamic behaviour is thereby largely determined by the surrounding structure. Therefore the frequency response of the entire measuring arrangement must be investigated for the largest possible, useful measuring range.

There are two possibilities here: frequency analysis, f.e. pressure sensors in shock tube or finite-element method.

 
 
Kistler Italy is
a member of...
KIT_member of Rev1


Press modules
KIT_Pressa
Electromechanical NC Press-Fit Systems with Piezoelectric Force Monitoring.
More informations

Kistler View 2012

Alleanza Kistler-Leane
Leane International
Distributore in esclusiva per il mercato italiano della linea di prodotti Vehicle RoaDyn
more...

Kistler Italy is an ISO 9001:2000 certified company
Kit SQS logo


Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +39 02 481 2751