Plastics




Fundamentals of Mold Cavity Pressure Measurement

The cavity pressure within an injection mold provides very precise information about the filling phase, the compression phase and the holding pressure phase.

The cavity pressure profile

The Cavity Pressure Curve
At the onset of the filling phase (1) the melt enters the cavity. As soon as the flow front reaches the sensor (2), pressure is registered. The pressure should rise in a near-linear gradient parallel to the duration of the filling time. At volumetric filling of the cavity, the filling phase has been completed (3) and the melt is compacted during the compression phase to ensure the forming of the contours of the mold cavity. The holding pressure phase follows after the maximum cavity pressure has been reached (4). The holding pressure phase compensates for the high thermal contraction of the polymer material – i.e., the reduction of its volume following the cooling down process – by introducing more material. During this phase, up to 10 % of the part volume is being pushed into the cavity. The fact that the molded part starts to cool down and solidify near the cavity wall inhibits the pressure transfer. The melt flow from the screw antechamber to the cavity is slowed down as the viscosity of the material increases and the flow channel becomes more constricted in the process. The progressive solidification of the melt (5) and the progressive thermal contraction causes the pressure within the cavity to drop to ambient levels (6).

The different characteristics of the molten amorphous and semi-crystalline plastics make no difference during the filling phase as long as their viscosities are identical and their compressibility factors are different. With semi-crystalline materials, more melt must be added to the mold in order to increase the pressure at the start of the holding pressure phase than is required with amorphous materials. While the plastic is cooling down under holding pressure, additional melt should be injected into the mold in order to compensate for the volume contraction and to prevent sink marks on the finished part.

Specific characteristics of amorphous thermoplastics

Specific Characteristics of Amorphous Thermoplastics
During the holding pressure phase of injection molding processes involving amorphous polymers such as polystyrene (PS), acrylonitrile-butadiene-styrene (ABS), styrene-acrylo-nitrile (SAN), polymethyl methacrylate (PMMA), polycarbonate (PC) and polyvinyl chloride (PVC), the mold cavity pressure drops to ambient pressure levels parallel to the declining part temperature due to increasing viscosity and the corresponding deterioration of the pressure transfer from the screw antechamber.

Specific characteristics of semi-crystalline thermoplastics
Specific Characteristics of Semi-Crystalline Thermoplastics
Due to an initially sufficient pressure transfer during injection molding processes involving semi-crystalline materials such as polyethylene (PE), polypropylene (PP), polyamide (PA) and polyoxymethylene (POM) there is almost no change in mold cavity pressure during the period following the compression phase until the crystalline melting point is reached . After that, however, the significant volume contraction during crystallization brings about a steep drop in the pressure. The duration of the holding pressure phase depends on factors such as the wall thickness of the molded part, the degree of crystallization and the processing parameters. The crystalline melting point of semicrystalline materials, for example, is dependent on the prevailing cavity pressure.
 
 
Kistler Italy is
a member of...
KIT_member of Rev1


QualityMolding
Logo_QualityMolding_Teaser_110.gif
Quality Molding is the 100% quality seal for injection molding processes.
more...

News 29.10.2010
Img_clearpixel
Kistler and STASA develop an automatic method for the prognosis of injection molded part quality
more...

Press modules
KIT_Pressa
Electromechanical NC Press-Fit Systems with Piezoelectric Force Monitoring.
More informations

Kistler Italy is an ISO 9001:2000 certified company
Kit SQS logo


Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +39 02 481 2751