Glossary
Accuracy class
The accuracy class of a Kistler sensor is determined by the maximum value of specified influence quantities (in percentage), however, a tolerance in characteristic value is not taken into account: • temperature impact on characteristic value (per 10 K) • temperature impact on zero point (per 10 K) • repeatability • linearity including hysteresis Note: accuracy class does not correspond to the classification scheme according to the guidelines EN ISO 376 or DIN 51309.
|