Mold trial or, to be more exact, the acceptance of molded parts for large-scale production, is a time-consuming process for molders. In this development phase, cavity pressure measurement systems can be used to analyze the process and to determine initial machine settings based on the relevant process parameter and without mold filling studies. Moreover, the cavity pressure signal is an important tool for uncovering errors and problems at an early stage, which also minimizes the number mold modifications required. Practical experience shows that mold cavity pressure systems can reduce the time and effort used for mold trial by up to 75 %.
|