Plastics




Kistler Drift Compensation

Drift compensation is an integral part of the charge amplifier
Drift compensation is an integral part of the charge amplifier.

”Drift” in piezoelectric measurement is a gradual variation of the measured value. It is caused by the way the actual charge amplifier (charge-to-voltage converter) works, but also results from thermal effects and finite resistances in the sensor and connecting cables. In typical  applications electrical and thermal drift occurs slowly.

comparison: with/without drift compensation

A so called ”Drift Compensation” feature is eliminating this effect. The charge signals in the amplifier resulting from electrical and thermal drift are detected and appropriate compensation applied. It therefore ensures that on the one hand the analog output signal of the change amplifier remains within a defined range of values, and on the other hand an accurate and stable measurement signal is available even when measuring over long periods of time.

Switchable drift compensation is now a standard function of Kistler charge amplifiers. Together with PiezoSmart automatic sensor identification, it represents a new standard in charge amplifier technology for engine indication.

 
 
QualityMolding
Logo_QualityMolding_Teaser_110.gif
Quality Molding is the 100% quality seal for injection molding processes.
more...

News 29.10.2010
Img_clearpixel
Kistler and STASA develop an automatic method for the prognosis of injection molded part quality
more...

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +44 1256 741 550