Manufacturing




Spot Welding

The quality of resistance spot welding is heavily influenced by the electrode clamping force and the weld current timing. Reliable process control therefore requires an effective and reliable monitoring system. The measurement solution is critical to the quality of this system. Kistler provides a series of alternatives, which on the one hand offer the possibility of measuring the electrode closing force indirectly, i.e. though the strain undergone by parts of the electrodes (sleeves) or the machine structure, or on the other hand directly between the electrodes.

Force measurement with strain sensor

Online process monitoring on static welding machines
A welding machine can be very easily retrofitted with Kistler piezoelectric force-strain sensors. The measuring point can be on the armature, near the electrode, or at a suitable point on the frame of the machine.

For specialized machines or welding systems with special electrode designs (e.g. projection welding machines), and for dimensional reasons, there is the option of measuring force with integrated load washers. This involves mounting one or more force sensors in machine components such as flanges, in connecting rods of pneumatic or electric servomotors, or behind platen type electrodes.

The picture on the left hand side shows an indirect force measurement with a Kistler strain sensor, Typ 9232.

Electrode force measurement

Direct in-situ electrode force measurement (calibration) on welding guns and welding machines
Robot spot welding guns have to be tested during product development in order to test methods or measure and check operation after installation. The electrode clamping force can be calibrated with an extremely high level of repeatability with the Typ 9831... welding force calibration transmitter as reference unit. The piezoelectric force sensor's high factor of safety against overload is also a considerable advantage, since on test rigs, for example, the electrodes can meet asymmetrically, giving rise to high impact forces.

Force measurement

Offline force measurement in cap milling stations
Late detection of defects in the resistance spot welding guns used in body construction or of incorrect process parameters can lead to costly production rejects. The Typ 9833... welding force test transmitter was designed for regular force measurement on production lines. The welding robots test the electrode force automatically on the basis of the number of cycles and load. The force measurement system is integrated into a service station, and during operation the welding robot runs through a regular service cycle involving re-milling the electrode caps as required.


» Direct access to the Product Finder, Manufacturing

 
 
Maximum
XY Monitoring

CAD Download
Kistler CAD Download Service
Kistler CAD Download Service Brings Sensors and Electronics Straight into Design
more...

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +358 9 612 1566