Setup and Service

When setting up and servicing mold cavity pressure sensors the following three steps are important: insulation testing, sensitivity testing and repair of the single-wire cables.
|
Insulation TestingPressure sensors are maintenance-free, however the insulation should be checked during a mold service. The following instructions must be observed:
• Ensure the connector is dry • When cleaning, cover the mounting bore or keep it clean • Use cleaning spray Type 1003 • Check insulation with the tester Type 5493: Reference value >1013 Ω » Troubleshooting
Sensor SensitivityAn incorrect installation of a sensor affects its sensitivity. The sensitivity of an installed sensor must therefore be tested, if possible before setting up the mold on the machine.
• Test the sensitivity of the sensor with the set Type 5993A...
» Troubleshooting
Repair of Single-Wire CablesRepair slight damage to the cable with repair kit Type 1207. Solder broken cables and cover joint with Teflon sheath and heat-shrink tubing of the repair kit Type 1207.
» Single-Wire cable repair
|
|
|

Quality Molding is the 100% quality seal for injection molding processes.
more...

Quality Monitoring and Process Control for Injection Molding Processes Download PDF

Kistler and STASA develop an automatic method for the prognosis of injection molded part quality
more...
|