Kistler - measure. analyse. innovate.
   
|Home |Search |Contact |Sitemap |Login/Registration | |Deutsch |Français |
 
crosshair left crosshair right
spacer
spacer
spacer
spacer
spacer
spacer
 
Measuretape
 
spacer
  Plastics




Minimal Process Variation with Real-Time Control

Automatic switchover from injection to holding pressure and cascade control are just two examples of how cavity pressure is used for real-time process control. The extremely dynamic characteristics of cavity pressure sensors enable the process to be controlled with great precision and to respond to changes promptly while the process is still ongoing.

Switching over from the injection phase to the holding pressure phase

Switching over from the injection phase to the holding pressure phase is the method used most frequently. Most injection molding machines with cavity pressure measurement feature this type of switchover as an integrated function. The switchover is actuated not by the screw position or the injected volume but by a threshold value for cavity pressure. In this way, the effects of viscosity and metering fluctuations on the switchover point are minimized. In addition to switching over at a specific pressure, it is also possible to use an intelligent system for the purpose of the switchover. Such systems automatically detect volumetric cavity filling and send a signal instructing the injection machine to switch over from injection to holding pressure. During injection these systems analyze the cavity pressure curve and detect the characteristic rise in pressure that occurs on transition from the filling phase to the compression phase.

Cascade control
Cascade control based on cavity pressure sensors enables the process to be optimized efficiently with these complex systems, and to ensure consistent filling in production even when process fluctuations occur. More than one sensor may be located in the mold according to the number of gares and the geometry of the molded part. The position of the flow front or fronts can be detected by the sensors and the appropriate gares can be opened.
Screw antechamber pressure, mold way and mold cavity pressure

Cavity pressure sensors are also used in the control of special processes in order to minimize process fluctuations. With fluid injection technology (GAIM and WIT), introduction of the fluid is started when the mold cavity pressure has reached the relevant level; a delay time is taken into account.

The switchover from injection to compression in an injection compression molding process can be performed in various ways, using the screw position, the injection volume or also a force that is exerted by the melt on the embossing stamp, for instance. Especially in cases where the surfaces are more complex, the switchover point must be exactly right if undesirable marks are to be avoided. In this type of process, too, using mold cavity pressure to determine the switchover point leads to consistently high quality in the molded parts.

 
 
QualityMolding
Logo_QualityMolding_Teaser_110.gif
Quality Molding is the 100% quality seal for injection molding processes.
more...

Sensors and Systems
Sensors and Systems (PDF)
Quality Monitoring and Process Control for Injection Molding Processes
Download PDF

News 29.10.2010
Img_clearpixel
Kistler and STASA develop an automatic method for the prognosis of injection molded part quality
more...

Top Top
Recommend page| Print| Disclaimer| Trademarks| Webmaster| e-Contact| +41 52 224 11 11